Working of srktool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Working of srktool

1,097件の閲覧回数
shashank_r
Contributor I

Hi...
I was learning the Code signing for secure boot. I referred the CST User guide document. In that, I require clarification of 1 step.

I am working on HAB4. I have generated the SRK keys and certificates using the ./hab4_pki_tree.sh script. Now the second part, creating the fuse.bin and table.bin using srktool. I have generated them as well with srktool, the thing I want to know here is,
Q1. what is the hash that is stored in fuse.bin, by that I mean what structure of hashing is followed (is it concatenation, binary tree format - merkle tree). Show me steps so that I can manually create the hash and verify it against the one crteated by the tool.
Q2. What is the structure of the table.bin file. I mean what it contains, by table I assume it should have some rows and columns, what are they ?

0 件の賞賛
返信
2 返答(返信)

1,063件の閲覧回数
shashank_r
Contributor I

So.. should I have to raise a new request in the iMX Processor forum, or can this be forwarded or tagged to them ?

0 件の賞賛
返信

1,070件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi,

 

CST is not part of MCUXpresso Config Tools and probably no one will reply here. CST is frequently discussed in this forum.

 

Regards,

Libor

0 件の賞賛
返信