Working of srktool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Working of srktool

1,208 Views
shashank_r
Contributor I

Hi...
I was learning the Code signing for secure boot. I referred the CST User guide document. In that, I require clarification of 1 step.

I am working on HAB4. I have generated the SRK keys and certificates using the ./hab4_pki_tree.sh script. Now the second part, creating the fuse.bin and table.bin using srktool. I have generated them as well with srktool, the thing I want to know here is,
Q1. what is the hash that is stored in fuse.bin, by that I mean what structure of hashing is followed (is it concatenation, binary tree format - merkle tree). Show me steps so that I can manually create the hash and verify it against the one crteated by the tool.
Q2. What is the structure of the table.bin file. I mean what it contains, by table I assume it should have some rows and columns, what are they ?

0 Kudos
Reply
2 Replies

1,174 Views
shashank_r
Contributor I

So.. should I have to raise a new request in the iMX Processor forum, or can this be forwarded or tagged to them ?

0 Kudos
Reply

1,181 Views
liborukropec
NXP Employee
NXP Employee

Hi,

 

CST is not part of MCUXpresso Config Tools and probably no one will reply here. CST is frequently discussed in this forum.

 

Regards,

Libor

0 Kudos
Reply