Windows Embedded Compact 7 X-Loader for i.MX51

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows Embedded Compact 7 X-Loader for i.MX51

ソリューションへジャンプ
1,759件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about the X-Loader for i.MX51.

It includes the Windows Embedded CE 6.0 X-Loader for i.MX51 in BSP.

On the other hand, it does not include the Windows Embedded Compact 7 X-Loader for i.MX51 in BSP.

 

Q1.

How can we get the Windows Embedded Compact 7 X-Loader for i.MX51?

 

Best Regards,

Eishi SHIBUSAWA

 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,596件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NXP WinEC7 BSP does not use 3 stage boot technology : XLDR -> EBOOT -> NK,

assuming two stage : EBOOT->NK

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,597件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NXP WinEC7 BSP does not use 3 stage boot technology : XLDR -> EBOOT -> NK,

assuming two stage : EBOOT->NK

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信