Windows Embedded Compact 7 X-Loader for i.MX51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows Embedded Compact 7 X-Loader for i.MX51

Jump to solution
1,746 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to ask you about the X-Loader for i.MX51.

It includes the Windows Embedded CE 6.0 X-Loader for i.MX51 in BSP.

On the other hand, it does not include the Windows Embedded Compact 7 X-Loader for i.MX51 in BSP.

 

Q1.

How can we get the Windows Embedded Compact 7 X-Loader for i.MX51?

 

Best Regards,

Eishi SHIBUSAWA

 

Labels (2)
0 Kudos
Reply
1 Solution
1,583 Views
Yuri
NXP Employee
NXP Employee

Hello,

  NXP WinEC7 BSP does not use 3 stage boot technology : XLDR -> EBOOT -> NK,

assuming two stage : EBOOT->NK

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,584 Views
Yuri
NXP Employee
NXP Employee

Hello,

  NXP WinEC7 BSP does not use 3 stage boot technology : XLDR -> EBOOT -> NK,

assuming two stage : EBOOT->NK

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply