Windows CE porting to IMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows CE porting to IMX6Q

1,602件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have got IMX6 Reference board to which we have ported Ubuntu, Debian, Yocto etc. It is working fine. We also would like to test Windows CE on IMX6DL board.

Can anybody suggest from where to download Windows CE??? any technical documents available???

ラベル(2)
0 件の賞賛
返信
1 返信

1,420件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

Freescale does not support Windows CE on i.MX6 platform,

for Windows CE BSPs one can apply to partners, like Adeneo and others.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信