Windows CE porting to IMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows CE porting to IMX6Q

1,229 Views
srinivasaporam
Contributor II

Hi,

We have got IMX6 Reference board to which we have ported Ubuntu, Debian, Yocto etc. It is working fine. We also would like to test Windows CE on IMX6DL board.

Can anybody suggest from where to download Windows CE??? any technical documents available???

Labels (2)
0 Kudos
Reply
1 Reply

1,047 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

Freescale does not support Windows CE on i.MX6 platform,

for Windows CE BSPs one can apply to partners, like Adeneo and others.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply