Wifi Hotspot without sharing internet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Wifi Hotspot without sharing internet

跳至解决方案
1,617 次查看
amit251291
Contributor IV

Dear all,

We are working on i.MX.6 platform running on android 7.1.2. We have a requirement as below. 

"WiFi hotspot of i.MX.6 platform should not share the internet to connected mobile. i.MX.6 platform should use the internet connection only for itself."

We can not disable internet connection to satisfy this requirement because we need to send MQTT data to cloud always, even when hotspot is enabled. 

Is this kind of implementation possible ? If yes, how ? Can somebody throw light on this ?

Thank you so much in advance. 

标签 (2)
0 项奖励
回复
1 解答
1,511 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Amitt,

I understand this is not possible since it is how it is handle the Wifi Hot Spot from Android Services, you should ask in the Android Developer Community, if there is a way to modify this service or deamon since from our side, it is what it is expected to be.

I apologize for the inconvenience.

在原帖中查看解决方案

2 回复数
1,512 次查看
jamesbone
NXP TechSupport
NXP TechSupport

Hello Amitt,

I understand this is not possible since it is how it is handle the Wifi Hot Spot from Android Services, you should ask in the Android Developer Community, if there is a way to modify this service or deamon since from our side, it is what it is expected to be.

I apologize for the inconvenience.

1,511 次查看
amit251291
Contributor IV

Thank you jamesbone‌ for your response. 

0 项奖励
回复