Wifi Hotspot without sharing internet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wifi Hotspot without sharing internet

ソリューションへジャンプ
1,609件の閲覧回数
amit251291
Contributor IV

Dear all,

We are working on i.MX.6 platform running on android 7.1.2. We have a requirement as below. 

"WiFi hotspot of i.MX.6 platform should not share the internet to connected mobile. i.MX.6 platform should use the internet connection only for itself."

We can not disable internet connection to satisfy this requirement because we need to send MQTT data to cloud always, even when hotspot is enabled. 

Is this kind of implementation possible ? If yes, how ? Can somebody throw light on this ?

Thank you so much in advance. 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,503件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Amitt,

I understand this is not possible since it is how it is handle the Wifi Hot Spot from Android Services, you should ask in the Android Developer Community, if there is a way to modify this service or deamon since from our side, it is what it is expected to be.

I apologize for the inconvenience.

元の投稿で解決策を見る

2 返答(返信)
1,504件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Amitt,

I understand this is not possible since it is how it is handle the Wifi Hot Spot from Android Services, you should ask in the Android Developer Community, if there is a way to modify this service or deamon since from our side, it is what it is expected to be.

I apologize for the inconvenience.

1,503件の閲覧回数
amit251291
Contributor IV

Thank you jamesbone‌ for your response. 

0 件の賞賛
返信