Which one is right..?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which one is right..?

Jump to solution
2,429 Views
machlee
Contributor II

Hello...?

I am on working on image enhancement of i.MX6Q camera interfaces.

I have found some confusing on freescale's documents.

There are tow documents.

1. i.MX 6Dual/6Quad Linux Reference Manual, Rev. L3.0.35_1.1.0, 01/2013

2. i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 0, 11/2012

But the explanation of IPU block is different by each other,

especially ISP which is on between CSI and IDMAC described at Linux Reference Manual.

Can you let me know which one is right.. or some differences by Chip version or Chip series..?

Thank you in advance.

Mach.

Here it is the two block diagrams.

IPU_Linux_RM.JPGIPU_AP_RM.JPG

Labels (4)
0 Kudos
Reply
1 Solution
2,267 Views
Yuri
NXP Employee
NXP Employee

This is old story about the ISP :

On iMX5x IPU, there is a module called ISP, which was not fully verified, so in the iMX5x

documentation, the ISP section had been removed.  And on iMX6, the ISP module had been

removed.

View solution in original post

0 Kudos
Reply
2 Replies
2,268 Views
Yuri
NXP Employee
NXP Employee

This is old story about the ISP :

On iMX5x IPU, there is a module called ISP, which was not fully verified, so in the iMX5x

documentation, the ISP section had been removed.  And on iMX6, the ISP module had been

removed.

0 Kudos
Reply
2,267 Views
machlee
Contributor II

Thanks a lot  :-)

0 Kudos
Reply