Which one is right..?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which one is right..?

跳至解决方案
2,477 次查看
machlee
Contributor II

Hello...?

I am on working on image enhancement of i.MX6Q camera interfaces.

I have found some confusing on freescale's documents.

There are tow documents.

1. i.MX 6Dual/6Quad Linux Reference Manual, Rev. L3.0.35_1.1.0, 01/2013

2. i.MX 6Dual/6Quad Applications Processor Reference Manual, Rev. 0, 11/2012

But the explanation of IPU block is different by each other,

especially ISP which is on between CSI and IDMAC described at Linux Reference Manual.

Can you let me know which one is right.. or some differences by Chip version or Chip series..?

Thank you in advance.

Mach.

Here it is the two block diagrams.

IPU_Linux_RM.JPGIPU_AP_RM.JPG

标签 (4)
0 项奖励
回复
1 解答
2,315 次查看
Yuri
NXP Employee
NXP Employee

This is old story about the ISP :

On iMX5x IPU, there is a module called ISP, which was not fully verified, so in the iMX5x

documentation, the ISP section had been removed.  And on iMX6, the ISP module had been

removed.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,316 次查看
Yuri
NXP Employee
NXP Employee

This is old story about the ISP :

On iMX5x IPU, there is a module called ISP, which was not fully verified, so in the iMX5x

documentation, the ISP section had been removed.  And on iMX6, the ISP module had been

removed.

0 项奖励
回复
2,315 次查看
machlee
Contributor II

Thanks a lot  :-)

0 项奖励
回复