Where is the cross compile tool-chain

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Where is the cross compile tool-chain

跳至解决方案
1,677 次查看
dingzhang
Contributor III

I'm using the SABRD board with im6 Quad.

After compiling the Yocto_Project  xwayland: "bitbake fsl-image-qt5"

But where is the cross compile tool-chain??

Thanks a lot

标签 (3)
0 项奖励
回复
1 解答
1,411 次查看
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,412 次查看
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,411 次查看
dingzhang
Contributor III

Hi Yuri,

     Thanks for your reply.

     That helps ME a lot. according to your document, i bitbake the tool-chain and succeeded to cross compile my code.

     thanks again

ZHANG DING

0 项奖励
回复