Where is the cross compile tool-chain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the cross compile tool-chain

ソリューションへジャンプ
1,745件の閲覧回数
dingzhang
Contributor III

I'm using the SABRD board with im6 Quad.

After compiling the Yocto_Project  xwayland: "bitbake fsl-image-qt5"

But where is the cross compile tool-chain??

Thanks a lot

ラベル(3)
0 件の賞賛
返信
1 解決策
1,479件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,480件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

please refer to the following how to use the toolchain for NXP Linux BSP :

i.MX Yocto Project: How can I compile the kernel manually?

cannot find crt1.o

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,479件の閲覧回数
dingzhang
Contributor III

Hi Yuri,

     Thanks for your reply.

     That helps ME a lot. according to your document, i bitbake the tool-chain and succeeded to cross compile my code.

     thanks again

ZHANG DING

0 件の賞賛
返信