Hi,
The problem on imx6 sabresd_6dq with android 4.2.2 and kernel 3.0.35.
Log print out a lot of the follow contents:
W/MediaPlayer( 3976): info/warning (3, 0)
E/OMXCodec( 2254): [OMX.Freescale.std.video_decoder.avc.v3.hw-based] dequeueBuffer failed w/ error 0xfffffff0
I/MediaPlayer( 3976): Info (3,0)
Thanks.
Actually, this is the effect of some memory segmentation issue of the 3.0.35 kernel. Migrating to later BSP with later kernel revision should fix the issue.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------