When the IMX6 decoding AVC format is very high probability will be stuck?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When the IMX6 decoding AVC format is very high probability will be stuck?

1,968 次查看
fdact
Contributor I

Hi,

   The problem on imx6 sabresd_6dq  with android 4.2.2 and kernel 3.0.35.

   Log print out a lot of the follow contents:
   W/MediaPlayer( 3976): info/warning (3, 0)
   E/OMXCodec( 2254): [OMX.Freescale.std.video_decoder.avc.v3.hw-based] dequeueBuffer failed w/ error 0xfffffff0
   I/MediaPlayer( 3976): Info (3,0)

Thanks.

标签 (1)
0 项奖励
回复
3 回复数

1,754 次查看
art
NXP Employee
NXP Employee

Actually, this is the effect of some memory segmentation issue of the 3.0.35 kernel. Migrating to later BSP with later kernel revision should fix the issue.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,754 次查看
fdact
Contributor I

Can you kindly tell me which kernel version can be used on Android4.2.2? where to download? Can I only update kernel for my android system?

Thanks.

0 项奖励
回复

1,754 次查看
art
NXP Employee
NXP Employee

Q. Can I only update kernel for my android system?

A. No, it's not possible to only update the kernel. You have to completely migrate to later Android. Better to use the latest Marshmallow 6.0.1 BSP.

0 项奖励
回复