What is the maximum output resolution of lcd? (in i.mx8qx)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the maximum output resolution of lcd? (in i.mx8qx)

1,726 Views
yoonseok
Contributor III

What is the maximum output resolution of lcd? (in i.mx8qx)
At 1280 x 720 30 fps, it glitters.
At 800 x 600 30fps, it comes out normal.
Is this right?

0 Kudos
Reply
4 Replies

1,722 Views
igorpadykov
NXP Employee
NXP Employee

Hi  Yoonseok

 

supported resolutions can be found in sect.15.3.1.2 Features

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply

1,703 Views
yoonseok
Contributor III

Please ignore the questions below.

The LCD we want to use is The Parallel Display Interface (LCD).

Datasheet
"
15.1.1.1 Block Diagram

...
"The Parallel Display Interface (LCD Interface), which supports
720p60 display"
"

I'm sorry. I misrepresented the environment we tested.
Let me summarize the test results

Test Results
The Parallel Display Interface( LCD) (in i.mx8qx).
At 1280 x 720 60 fps, it glitters.
At 800 x 600 58fps, it comes out normal.

So we would like to test at 1280 x 720 resolution at 30fps.

What should I modify to change to 1280x720 60fps --> 30fps?

0 Kudos
Reply

1,713 Views
yoonseok
Contributor III

Additional Questions

What is the modification point when you make the following changes?

Lcd 720P 60fps --> 720P 30fps

0 Kudos
Reply

1,716 Views
yoonseok
Contributor III

Thank you for your answer.
What I want is about The Parallel Display Interface( LCD).

15.1.1.1 Block Diagram

...
"The Parallel Display Interface (LCD Interface), which supports 720p60 display"
It says,

But  The screen is shaking at 720P.

0 Kudos
Reply