What is the maximum output resolution of lcd? (in i.mx8qx)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the maximum output resolution of lcd? (in i.mx8qx)

1,678 次查看
yoonseok
Contributor III

What is the maximum output resolution of lcd? (in i.mx8qx)
At 1280 x 720 30 fps, it glitters.
At 800 x 600 30fps, it comes out normal.
Is this right?

0 项奖励
回复
4 回复数

1,674 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  Yoonseok

 

supported resolutions can be found in sect.15.3.1.2 Features

i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual

 

Best regards
igor

0 项奖励
回复

1,655 次查看
yoonseok
Contributor III

Please ignore the questions below.

The LCD we want to use is The Parallel Display Interface (LCD).

Datasheet
"
15.1.1.1 Block Diagram

...
"The Parallel Display Interface (LCD Interface), which supports
720p60 display"
"

I'm sorry. I misrepresented the environment we tested.
Let me summarize the test results

Test Results
The Parallel Display Interface( LCD) (in i.mx8qx).
At 1280 x 720 60 fps, it glitters.
At 800 x 600 58fps, it comes out normal.

So we would like to test at 1280 x 720 resolution at 30fps.

What should I modify to change to 1280x720 60fps --> 30fps?

0 项奖励
回复

1,665 次查看
yoonseok
Contributor III

Additional Questions

What is the modification point when you make the following changes?

Lcd 720P 60fps --> 720P 30fps

0 项奖励
回复

1,668 次查看
yoonseok
Contributor III

Thank you for your answer.
What I want is about The Parallel Display Interface( LCD).

15.1.1.1 Block Diagram

...
"The Parallel Display Interface (LCD Interface), which supports 720p60 display"
It says,

But  The screen is shaking at 720P.

0 项奖励
回复