What is the maximum output resolution of lcd? (in i.mx8qx)At 1280 x 720 30 fps, it glitters.At 800 x 600 30fps, it comes out normal.Is this right?
Hi Yoonseok
supported resolutions can be found in sect.15.3.1.2 Features
i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual
Best regardsigor
Please ignore the questions below.The LCD we want to use is The Parallel Display Interface (LCD).Datasheet"15.1.1.1 Block Diagram..."The Parallel Display Interface (LCD Interface), which supports720p60 display""I'm sorry. I misrepresented the environment we tested.Let me summarize the test resultsTest ResultsThe Parallel Display Interface( LCD) (in i.mx8qx).At 1280 x 720 60 fps, it glitters.At 800 x 600 58fps, it comes out normal.So we would like to test at 1280 x 720 resolution at 30fps.What should I modify to change to 1280x720 60fps --> 30fps?
Additional Questions
What is the modification point when you make the following changes?Lcd 720P 60fps --> 720P 30fps
Thank you for your answer.What I want is about The Parallel Display Interface( LCD).15.1.1.1 Block Diagram
..."The Parallel Display Interface (LCD Interface), which supports 720p60 display"It says,
But The screen is shaking at 720P.