What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

ソリューションへジャンプ
3,141件の閲覧回数
machengyuan
Contributor I

Hello,

What is the difference between Parameter Register's   Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ma

Parameter Register's (read only) shows sai configuration implemented in that processor:

for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32

This corresponds description for SAI Transmit Configuration 4 Register (TCR4):

"FRSZ -The maximum supported frame size is 32 words."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,010件の閲覧回数
machengyuan
Contributor I

Thank you very much!

0 件の賞賛
返信
3,010件の閲覧回数
machengyuan
Contributor I

Hi,

So Parameter Register's   Frame Size is only going to be 5 at most, even if it has 4 bits, right?

0 件の賞賛
返信
3,010件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Parameter Register shows what max. Frame Size is implemented in

that processor silicon sai module. In other processors silicons it may have other values.

Best regards
igor

0 件の賞賛
返信
3,011件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ma

Parameter Register's (read only) shows sai configuration implemented in that processor:

for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32

This corresponds description for SAI Transmit Configuration 4 Register (TCR4):

"FRSZ -The maximum supported frame size is 32 words."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信