What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the difference between Parameter Register's Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

Jump to solution
3,178 Views
machengyuan
Contributor I

Hello,

What is the difference between Parameter Register's   Frame Size and SAI Transmit Configuration 4 Register 's Frame Size?

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
3,047 Views
igorpadykov
NXP Employee
NXP Employee

Hi ma

Parameter Register's (read only) shows sai configuration implemented in that processor:

for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32

This corresponds description for SAI Transmit Configuration 4 Register (TCR4):

"FRSZ -The maximum supported frame size is 32 words."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,047 Views
machengyuan
Contributor I

Thank you very much!

0 Kudos
Reply
3,047 Views
machengyuan
Contributor I

Hi,

So Parameter Register's   Frame Size is only going to be 5 at most, even if it has 4 bits, right?

0 Kudos
Reply
3,047 Views
igorpadykov
NXP Employee
NXP Employee

Parameter Register shows what max. Frame Size is implemented in

that processor silicon sai module. In other processors silicons it may have other values.

Best regards
igor

0 Kudos
Reply
3,048 Views
igorpadykov
NXP Employee
NXP Employee

Hi ma

Parameter Register's (read only) shows sai configuration implemented in that processor:

for example FRAME (Frame Size) =5 : The maximum number of slots per frame is 2^FRAME: 32

This corresponds description for SAI Transmit Configuration 4 Register (TCR4):

"FRSZ -The maximum supported frame size is 32 words."

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply