What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is maximun resolution that i.MX6 Dual can manage with MiPi DSI?

跳至解决方案
1,487 次查看
jdepedro
Contributor IV

 Looking at the NXP documentation there is a mismatching or a typo, looking at the manuals:

"Programmable display resolutions, from 160x120(QQVGA) to 1280x720(XVGA)."

"Programmable display resolutions, from 160x120(QQVGA) to 1024x768(XVGA)"

Also seems like XVGA is not an standard format: wikipedia

Could you confirm what is the correct information? Thanks

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,212 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,213 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  "The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,

as specified in the Reference Manual document.

MIPI DSI max display resolution 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复