MIPI DSI max display resolution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIPI DSI max display resolution

ソリューションへジャンプ
4,433件の閲覧回数
jotes
Contributor IV

What is the maximum display resolution for MIPI DSI?

Is it 1280x720 (as it is mentioned in IMX6DQRM Rev. 3, 07/2015) or is it 1024x768 (IMX6QLXRM Rev L3.0.35_4.1.0, 09/2013)?

We would like to connect the 1280x720 Super AMOLED display to our IMX6Q board, and we wonder if it has any chance to work correctly?

ラベル(5)
0 件の賞賛
返信
1 解決策
3,301件の閲覧回数
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,302件の閲覧回数
art
NXP Employee
NXP Employee

The maximum possible display resolution on the MIPI DSI interface of the i.MX6Dual/Quad processors is 1280x720 pixels, as specified in the Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信