Looking at the NXP documentation there is a mismatching or a typo, looking at the manuals:
"Programmable display resolutions, from 160x120(QQVGA) to 1280x720(XVGA)."
"Programmable display resolutions, from 160x120(QQVGA) to 1024x768(XVGA)"
Also seems like XVGA is not an standard format: wikipedia
Could you confirm what is the correct information? Thanks
解決済! 解決策の投稿を見る。
Hello,
"The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,
as specified in the Reference Manual document.
MIPI DSI max display resolution
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
"The maximum possible display resolution on the MIPI DSI interface of the i.MX6 [...] is 1280x720 pixels,
as specified in the Reference Manual document.
MIPI DSI max display resolution
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------