What does interactive scaling governor do

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What does interactive scaling governor do

跳至解决方案
3,519 次查看
ranjithkumar_kv
Contributor II

Hi,

We are using i.MX8M Mini processor in our project. While checking the available frequency governors we had seen like there is a mode called "interactive".

Userspace mode will help the user to change the cpu frequency manually.

Ondemand mode will change the cpu frequency to maximum value automatically when the load is increased.

So like these modes how will the interactive scaling governor behaves? We had referred the reference manual also but we can not get a clear picture on how the interactive mode works.

Thanks

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,389 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can look at linux CPUfreq governor documentation

cpufreq.rst\pm\admin-guide\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
3,389 次查看
ranjithkumar_kv
Contributor II

Hi Igor,

Thank you for the information.

0 项奖励
回复
3,390 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can look at linux CPUfreq governor documentation

cpufreq.rst\pm\admin-guide\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------