What does interactive scaling governor do

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What does interactive scaling governor do

ソリューションへジャンプ
3,510件の閲覧回数
ranjithkumar_kv
Contributor II

Hi,

We are using i.MX8M Mini processor in our project. While checking the available frequency governors we had seen like there is a mode called "interactive".

Userspace mode will help the user to change the cpu frequency manually.

Ondemand mode will change the cpu frequency to maximum value automatically when the load is increased.

So like these modes how will the interactive scaling governor behaves? We had referred the reference manual also but we can not get a clear picture on how the interactive mode works.

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,380件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can look at linux CPUfreq governor documentation

cpufreq.rst\pm\admin-guide\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
3,380件の閲覧回数
ranjithkumar_kv
Contributor II

Hi Igor,

Thank you for the information.

0 件の賞賛
返信
3,381件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Ranjith

one can look at linux CPUfreq governor documentation

cpufreq.rst\pm\admin-guide\Documentation - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------