Do we need a R115 in i.MX6SLEVK ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do we need a R115 in i.MX6SLEVK ?

ソリューションへジャンプ
1,989件の閲覧回数
ko-hey
Senior Contributor II

Hi all,

I would like to know why a R115 in i.MX6SLEVK is needed.

Could someone tell me the reason for it ?

BR,

Kohei Tanaka

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,910件の閲覧回数
art
NXP Employee
NXP Employee

No, R115 is not mandatory required. Moreover, it is marked as DNP on the i.MX6SL EVK board schematic.

Best Regards,
Artur

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,911件の閲覧回数
art
NXP Employee
NXP Employee

No, R115 is not mandatory required. Moreover, it is marked as DNP on the i.MX6SL EVK board schematic.

Best Regards,
Artur

0 件の賞賛
返信
1,910件の閲覧回数
ko-hey
Senior Contributor II

Could someone follow this thread ?

Ko-hey

0 件の賞賛
返信