WIFI module which is compatible with 8MMINILPD4-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WIFI module which is compatible with 8MMINILPD4-EVK

ソリューションへジャンプ
1,947件の閲覧回数
joshua_hong
Contributor III

Hi,

 

do you have WIFI module / WIFI+Bluetooth compatible with 8MMINILPD4-EVK, other than the LBEE5ZZ1PJ-164 from Murata?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,855件の閲覧回数
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,856件の閲覧回数
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

0 件の賞賛
返信