WIFI module which is compatible with 8MMINILPD4-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

WIFI module which is compatible with 8MMINILPD4-EVK

跳至解决方案
1,988 次查看
joshua_hong
Contributor III

Hi,

 

do you have WIFI module / WIFI+Bluetooth compatible with 8MMINILPD4-EVK, other than the LBEE5ZZ1PJ-164 from Murata?

标签 (1)
0 项奖励
回复
1 解答
1,896 次查看
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,897 次查看
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

0 项奖励
回复