WIFI module which is compatible with 8MMINILPD4-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WIFI module which is compatible with 8MMINILPD4-EVK

Jump to solution
930 Views
joshua_hong
Contributor III

Hi,

 

do you have WIFI module / WIFI+Bluetooth compatible with 8MMINILPD4-EVK, other than the LBEE5ZZ1PJ-164 from Murata?

Labels (1)
0 Kudos
1 Solution
838 Views
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

View solution in original post

0 Kudos
1 Reply
839 Views
romitchatterjee
Contributor V

You can connect a 1CX module from Murata/Embedded Artists via the M.2 interface (on the back of the board). Its a 802.11 ac 2x2 MIMO module, with BT 5.0.

Here is the product page: 1CX M.2 Module - Embedded Artists 

0 Kudos