WEC2013 Display driver bring up issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

WEC2013 Display driver bring up issue

1,624件の閲覧回数
senthilj
Contributor I

We are porting WEC2013 for a Freescale IMX controller. The OS is up and scheduling is fine. We are now developing the display driver based on DDGPE. The driver seems loaded properly and we could successfully bring up the hardware part and test pattern shown in the driver is visible.

But WEC2013 home screen is not visible. We have enabled SYSGEN_MINGDI SYSGEN_MINGWES along with Default Theme and a Screen Configuration (800 x 480 Landscape). DirectDraw(SYSGEN_DDRAW) is also enabled. Tried with enabling / disabling display stub driver too. Still we could not screen the home screen. Anything else is needed?

We also tried running a test window application compiled as a sub-project. Though the application is up and running (based on debug prints), that window is not visible. Should we do anything else?

ラベル(3)
1 返信

1,433件の閲覧回数
justin_jiang
NXP Employee
NXP Employee

can you measure the waveform of the display port, the bitclk, Vsync, Hsync, data pin....?

This can check if the IPU display port work or not.