Vybrid -- Fuse Programming/Verification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vybrid -- Fuse Programming/Verification

2,099件の閲覧回数
dalelawson
Contributor I

Is there a way to use a serial programming interface to burn the programmable fuses. This interface is enabled by default and is part of the ROM code run at startup by the processor. It is possible to use this interface to read back the register/fuse values.

In addition, are there any commercial programmers that have the capability of programming/verifying fuse configurations?

0 件の賞賛
返信
2 返答(返信)

1,835件の閲覧回数
dalelawson
Contributor I

There is no SPI flash component on the socket board to save the boot code to boot or
initial the device for efuse programming.

Can you advise is there any other way to program
the eFuse via direct signal control?

0 件の賞賛
返信

1,835件の閲覧回数
b36401
NXP Employee
NXP Employee

You can use u-boot to burn the fuses.

https://community.nxp.com/docs/DOC-95248

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信