Vybrid -- Fuse Programming/Verification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vybrid -- Fuse Programming/Verification

2,028 次查看
dalelawson
Contributor I

Is there a way to use a serial programming interface to burn the programmable fuses. This interface is enabled by default and is part of the ROM code run at startup by the processor. It is possible to use this interface to read back the register/fuse values.

In addition, are there any commercial programmers that have the capability of programming/verifying fuse configurations?

0 项奖励
回复
2 回复数

1,764 次查看
dalelawson
Contributor I

There is no SPI flash component on the socket board to save the boot code to boot or
initial the device for efuse programming.

Can you advise is there any other way to program
the eFuse via direct signal control?

0 项奖励
回复

1,764 次查看
b36401
NXP Employee
NXP Employee

You can use u-boot to burn the fuses.

https://community.nxp.com/docs/DOC-95248

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复