Using library compiled for ARM926EJ-S - MontaVista Linux 5.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using library compiled for ARM926EJ-S - MontaVista Linux 5.0

1,839件の閲覧回数
rans
Senior Contributor I

Hello,

I need to use imx6 with a device (cryptomemory) which is supplied with a library which was compiled for for  ARM926EJ-S - MontaVista Linux 5.0 .

Should it work with imx6 ?

This is the link for the cryptomemory device:

CryptoMemory Development Library 

Best Regards,

Ran

0 件の賞賛
返信
3 返答(返信)

1,756件の閲覧回数
art
NXP Employee
NXP Employee

The library, built for the ARM926EJ-S core and MontaVista Linux 5.0 is not guaranteed to work at all on the i.MX6's ARM Cortex A9 core and current Linux BSP. It would be better to get this library in source and then rebuild it with appropriate toolchain.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,756件の閲覧回数
rans
Senior Contributor I

Hi Artur,

I am not sure I can will get the source code.

Is there a slight chance that the compiled library will run with imx6 ?

Thanks,

Ran

0 件の賞賛
返信

1,756件の閲覧回数
art
NXP Employee
NXP Employee

I'm not sure. You can try it on your own risk.

0 件の賞賛
返信