Using iMX287 for the Street Light Control System

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using iMX287 for the Street Light Control System

1,433件の閲覧回数
linda_zhang
Contributor IV

We are using the i.MX287 chip for a street light control system project as this CPU can support industrial temperature operation and with speed up to 454MHz and low-cost. And we already used our MYD-IMX28X development board for evaluation. Share some photos with you.

image1.jpg

The board has rich peripherals including 2 x Ethernet, 2 x Serial ports, USB Host/Device, CAN, RS485, TF card slot, LCD, Audio…

image2.jpg

The MYC-IMX28X CPU module is compact with integrated i.MX287 CPU, 128MB DDR2, 256MB Nand Flash, 128KB SPI Flash and Ethernet PHY. The CPU module is only USD39/pc for MOQ1pc.

image3.jpg

Above image shows the QT interface on the 7” LCD display. The logo can be changed to your own.

image4.jpg

You can know more about this product from MYIR’s website:

  http://www.myirtech.com/list.asp?id=472

ラベル(3)
0 件の賞賛
返信
0 返答(返信)