Using iMX287 for the Street Light Control System

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using iMX287 for the Street Light Control System

1,408 Views
linda_zhang
Contributor IV

We are using the i.MX287 chip for a street light control system project as this CPU can support industrial temperature operation and with speed up to 454MHz and low-cost. And we already used our MYD-IMX28X development board for evaluation. Share some photos with you.

image1.jpg

The board has rich peripherals including 2 x Ethernet, 2 x Serial ports, USB Host/Device, CAN, RS485, TF card slot, LCD, Audio…

image2.jpg

The MYC-IMX28X CPU module is compact with integrated i.MX287 CPU, 128MB DDR2, 256MB Nand Flash, 128KB SPI Flash and Ethernet PHY. The CPU module is only USD39/pc for MOQ1pc.

image3.jpg

Above image shows the QT interface on the 7” LCD display. The logo can be changed to your own.

image4.jpg

You can know more about this product from MYIR’s website:

  http://www.myirtech.com/list.asp?id=472

Labels (3)
0 Kudos
Reply
0 Replies