Using Segger j-link with IMX8M plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using Segger j-link with IMX8M plus

Jump to solution
6,215 Views
niklasbergdahl
Contributor I

Are there any device-files to use with segger when debugging the M7 of an IMX8M Plus?
I'm trying to debug the M7 of an i.MX 8M Plus EVK, but run into trouble when trying to connect and reset.

Tags (1)
0 Kudos
Reply
1 Solution
6,210 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
4,708 Views
illy777
Contributor III

Hi there, is there an updated solution, because this doesn't work properly or I'm doing something wrong.

 

I'm on Windows 10, using the J-Flash 7.86 version: There is no support for the MIMX8MPRM devices.. I alredy did what the readme of the file above told and also tried downloading the instructions of the J-Link page - debugger starter kit. 

Therefore I put the files in following order in the %APPDATA%/../SEGGER-folder:

illy777_0-1680074546263.pngilly777_0-1680074546263.png

I also changed the .xml file:

illy777_1-1680074600551.pngilly777_1-1680074600551.png

It would help me a lot if anyone know further details or can reach me a hand!

 

Thank you!

 

 

 

 

0 Kudos
Reply
6,211 Views
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 Kudos
Reply