Using Segger j-link with IMX8M plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Using Segger j-link with IMX8M plus

跳至解决方案
4,866 次查看
niklasbergdahl
Contributor I

Are there any device-files to use with segger when debugging the M7 of an IMX8M Plus?
I'm trying to debug the M7 of an i.MX 8M Plus EVK, but run into trouble when trying to connect and reset.

标记 (1)
0 项奖励
回复
1 解答
4,861 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,359 次查看
illy777
Contributor III

Hi there, is there an updated solution, because this doesn't work properly or I'm doing something wrong.

 

I'm on Windows 10, using the J-Flash 7.86 version: There is no support for the MIMX8MPRM devices.. I alredy did what the readme of the file above told and also tried downloading the instructions of the J-Link page - debugger starter kit. 

Therefore I put the files in following order in the %APPDATA%/../SEGGER-folder:

illy777_0-1680074546263.png

I also changed the .xml file:

illy777_1-1680074600551.png

It would help me a lot if anyone know further details or can reach me a hand!

 

Thank you!

 

 

 

 

0 项奖励
回复
4,862 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Niklas

 

one can try IAR and SEGGER tool patch for i.MX8M Plus devices

and SDK_EVK-MIMX8MP available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 项奖励
回复