Using CLK pin for RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CLK pin for RTC

ソリューションへジャンプ
2,418件の閲覧回数
kbell_hardware
Contributor III

Hello,

I'm wondering if it is possible to not use the XTAL pins for your RTC clock input, but instead use the CLK1_P or CLK2_P pin. Using the IMX6Q

Thanks,

Kevin

ラベル(2)
0 件の賞賛
返信
1 解決策
2,168件の閲覧回数
LinWang
NXP Employee
NXP Employee


Hi Kevin,

They are impossible to be acted as RTC function.

1. There is no path from CLK1_N/P and CLK2_N/P to RTC block.

2. CLK1_N/P and CLK2_N/P pins belong to VDD_HIGH_CAP power group not VDD_SNVS_IN.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,169件の閲覧回数
LinWang
NXP Employee
NXP Employee


Hi Kevin,

They are impossible to be acted as RTC function.

1. There is no path from CLK1_N/P and CLK2_N/P to RTC block.

2. CLK1_N/P and CLK2_N/P pins belong to VDD_HIGH_CAP power group not VDD_SNVS_IN.

0 件の賞賛
返信