Using CLK pin for RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using CLK pin for RTC

Jump to solution
2,561 Views
kbell_hardware
Contributor III

Hello,

I'm wondering if it is possible to not use the XTAL pins for your RTC clock input, but instead use the CLK1_P or CLK2_P pin. Using the IMX6Q

Thanks,

Kevin

Labels (2)
0 Kudos
Reply
1 Solution
2,311 Views
LinWang
NXP Employee
NXP Employee


Hi Kevin,

They are impossible to be acted as RTC function.

1. There is no path from CLK1_N/P and CLK2_N/P to RTC block.

2. CLK1_N/P and CLK2_N/P pins belong to VDD_HIGH_CAP power group not VDD_SNVS_IN.

View solution in original post

0 Kudos
Reply
1 Reply
2,311 Views
LinWang
NXP Employee
NXP Employee


Hi Kevin,

They are impossible to be acted as RTC function.

1. There is no path from CLK1_N/P and CLK2_N/P to RTC block.

2. CLK1_N/P and CLK2_N/P pins belong to VDD_HIGH_CAP power group not VDD_SNVS_IN.

0 Kudos
Reply