Use 3.3V PWM in i.MX6SL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use 3.3V PWM in i.MX6SL

跳至解决方案
1,334 次查看
ko-hey
Senior Contributor II

Hi all,

 

My customer's using i.MX6SL and we have questions about PWM.

 

Q1.

They use HSIC_STROBE pad as a PWM2.

According to the datasheet, the pad's power group is NVCC_1P25.

https://www.nxp.com/docs/en/data-sheet/IMX6SLCEC.pdf

 

We believe that it's wrong and correct power group is NVCC_1P2V.

 

On the other hand, according to the i.MX Pins Tool v6, the pad is in NVCC_GPIO power group and it can select both 1.8V and 3.3V.

Which power group is correct ?

 

Q2.

If power group of the pad is NVCC_GPIO, the PWM can output 3.3V level ?

 

Ko-hey

 

标签 (3)
标记 (1)
0 项奖励
回复
1 解答
1,259 次查看
art
NXP Employee
NXP Employee

Actually, the HSIC_DATA and HSIC_STROBE signals are in the 1P2V power group. If you need to output 3.3V PWM signal, please select some other IOMUX option for the PWM2_OUT signal according to the Table 36-1 of the i.MX6SoloLite Reference manual document.

Best Regards,
Artur

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,260 次查看
art
NXP Employee
NXP Employee

Actually, the HSIC_DATA and HSIC_STROBE signals are in the 1P2V power group. If you need to output 3.3V PWM signal, please select some other IOMUX option for the PWM2_OUT signal according to the Table 36-1 of the i.MX6SoloLite Reference manual document.

Best Regards,
Artur

0 项奖励
回复