Use 3.3V PWM in i.MX6SL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use 3.3V PWM in i.MX6SL

Jump to solution
1,095 Views
ko-hey
Senior Contributor II

Hi all,

 

My customer's using i.MX6SL and we have questions about PWM.

 

Q1.

They use HSIC_STROBE pad as a PWM2.

According to the datasheet, the pad's power group is NVCC_1P25.

https://www.nxp.com/docs/en/data-sheet/IMX6SLCEC.pdf

 

We believe that it's wrong and correct power group is NVCC_1P2V.

 

On the other hand, according to the i.MX Pins Tool v6, the pad is in NVCC_GPIO power group and it can select both 1.8V and 3.3V.

Which power group is correct ?

 

Q2.

If power group of the pad is NVCC_GPIO, the PWM can output 3.3V level ?

 

Ko-hey

 

Labels (3)
Tags (1)
0 Kudos
Reply
1 Solution
1,020 Views
art
NXP Employee
NXP Employee

Actually, the HSIC_DATA and HSIC_STROBE signals are in the 1P2V power group. If you need to output 3.3V PWM signal, please select some other IOMUX option for the PWM2_OUT signal according to the Table 36-1 of the i.MX6SoloLite Reference manual document.

Best Regards,
Artur

View solution in original post

0 Kudos
Reply
1 Reply
1,021 Views
art
NXP Employee
NXP Employee

Actually, the HSIC_DATA and HSIC_STROBE signals are in the 1P2V power group. If you need to output 3.3V PWM signal, please select some other IOMUX option for the PWM2_OUT signal according to the Table 36-1 of the i.MX6SoloLite Reference manual document.

Best Regards,
Artur

0 Kudos
Reply