Updating u-boot and file system in u-boot cmd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating u-boot and file system in u-boot cmd

ソリューションへジャンプ
1,050件の閲覧回数
JHY
Contributor IV

How can I update u-boot image in u-boot console?

Linux kernel and dtb file are referenced in i.MX_Linux_User's_Guide.pdf, but u-boot image and file system are not.

In addition, SD card can update in host PC, but EMMC can only with MFGtool. Is it right?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
894件の閲覧回数
Yuri
NXP Employee
NXP Employee

   U-boot after load is working in DRAM, therefore new updated

version of U-boot may be loaded and written in the same manner as

kernel and dtb. Please refer to ucl2.xml file from MFG what is location

of U-boot image on selected media (SD, NAND).

Note :   MFG is the most preferable way to deploy images.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
895件の閲覧回数
Yuri
NXP Employee
NXP Employee

   U-boot after load is working in DRAM, therefore new updated

version of U-boot may be loaded and written in the same manner as

kernel and dtb. Please refer to ucl2.xml file from MFG what is location

of U-boot image on selected media (SD, NAND).

Note :   MFG is the most preferable way to deploy images.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信