Updating u-boot and file system in u-boot cmd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Updating u-boot and file system in u-boot cmd

Jump to solution
1,105 Views
JHY
Contributor IV

How can I update u-boot image in u-boot console?

Linux kernel and dtb file are referenced in i.MX_Linux_User's_Guide.pdf, but u-boot image and file system are not.

In addition, SD card can update in host PC, but EMMC can only with MFGtool. Is it right?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
949 Views
Yuri
NXP Employee
NXP Employee

   U-boot after load is working in DRAM, therefore new updated

version of U-boot may be loaded and written in the same manner as

kernel and dtb. Please refer to ucl2.xml file from MFG what is location

of U-boot image on selected media (SD, NAND).

Note :   MFG is the most preferable way to deploy images.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
950 Views
Yuri
NXP Employee
NXP Employee

   U-boot after load is working in DRAM, therefore new updated

version of U-boot may be loaded and written in the same manner as

kernel and dtb. Please refer to ucl2.xml file from MFG what is location

of U-boot image on selected media (SD, NAND).

Note :   MFG is the most preferable way to deploy images.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply