Unreal engine support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unreal engine support

4,698 Views
baishao
Contributor I

Hi,

I am wondering if NXP is now having any official demo running the unreal engine with imx? All i found is following:

Solved: IMX8 Unreal andVulkan Error - NXP Community

My understanding is that, by supporting vulkan, imx8/9 should be able to run unreal engine. But so far, never see a real example.

Thank you

0 Kudos
Reply
6 Replies

4,663 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

We have customer can run GPU/Vulkan app at i.MX8MP + Android 11.0.0_2.6.0 platform successfully .

While, there has no official released unreal engine example. 

Sorry for that may bring any inconvenience.

Mike

0 Kudos
Reply

4,646 Views
baishao
Contributor I

Hi Mike, thx for the reply. Is Vulkan driver included in standard yocto Linux build already? Or I need to build with a specific image to include it? I am currently building with “imx-image-multimedia”. Thank you 

0 Kudos
Reply

4,644 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer latest i.MX Yocto Linux BSP v6.6.52_2.2.0 release note with below info:

Hui_Ma_0-1735092828987.png

Wish it helps.

Mike

0 Kudos
Reply

4,611 Views
baishao
Contributor I

Thank you Mike. Based on following document:

https://www.nxp.com/docs/en/user-guide/IMX_GRAPHICS_USERS_GUIDE.pdf

It seems that IMX8 nano, and IMX95 also support Vulkan. However, these two devices are not shown in the Linux release note, the list that you showed. Would you please help to confirm if these two devices are currently supported?

0 Kudos
Reply

4,590 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

You are right. I.MX8M Nano and I.MX95 also support Vulkan 1.3 driver.

I had confirmed with i.MX product team that the Yocto release note has document issue missing both product with Table 8 about GPU relevant content.

We will follow up to correct that release note.

Mike

0 Kudos
Reply

4,578 Views
baishao
Contributor I

Thank you Mike.

0 Kudos
Reply