Unreal engine support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unreal engine support

4,732件の閲覧回数
baishao
Contributor I

Hi,

I am wondering if NXP is now having any official demo running the unreal engine with imx? All i found is following:

Solved: IMX8 Unreal andVulkan Error - NXP Community

My understanding is that, by supporting vulkan, imx8/9 should be able to run unreal engine. But so far, never see a real example.

Thank you

0 件の賞賛
返信
6 返答(返信)

4,697件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

We have customer can run GPU/Vulkan app at i.MX8MP + Android 11.0.0_2.6.0 platform successfully .

While, there has no official released unreal engine example. 

Sorry for that may bring any inconvenience.

Mike

0 件の賞賛
返信

4,680件の閲覧回数
baishao
Contributor I

Hi Mike, thx for the reply. Is Vulkan driver included in standard yocto Linux build already? Or I need to build with a specific image to include it? I am currently building with “imx-image-multimedia”. Thank you 

0 件の賞賛
返信

4,678件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer latest i.MX Yocto Linux BSP v6.6.52_2.2.0 release note with below info:

Hui_Ma_0-1735092828987.png

Wish it helps.

Mike

0 件の賞賛
返信

4,645件の閲覧回数
baishao
Contributor I

Thank you Mike. Based on following document:

https://www.nxp.com/docs/en/user-guide/IMX_GRAPHICS_USERS_GUIDE.pdf

It seems that IMX8 nano, and IMX95 also support Vulkan. However, these two devices are not shown in the Linux release note, the list that you showed. Would you please help to confirm if these two devices are currently supported?

0 件の賞賛
返信

4,624件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

You are right. I.MX8M Nano and I.MX95 also support Vulkan 1.3 driver.

I had confirmed with i.MX product team that the Yocto release note has document issue missing both product with Table 8 about GPU relevant content.

We will follow up to correct that release note.

Mike

0 件の賞賛
返信

4,612件の閲覧回数
baishao
Contributor I

Thank you Mike.

0 件の賞賛
返信