Unable to flash on custom imx8ulp board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to flash on custom imx8ulp board

28,857 Views
dhruvinrajpura
Contributor III

Hello,

Earlier I was using imx8ulp-evk9 to flash in that I was using uuu tool and with that I was able to generate flash.bin and can flash with below command
sudo uuu -V -b emmc flash.bin

 

Than I made custom board in which I am using chip MIMX8UD5D08SC and I am trying to flash with same command but after 29% uuu getting aborted.

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Wait for Known USB Device Appear...


Success 0    Failure 1                                                                                                                               
                                                                                                                                                      
                                                                                                                                                      
1:1      1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE         ] SDPS: boot -f /imx-mkimage/iMX8ULP/flash.bin 

 

Any changes I required to do if I am flashing on new board , I just want to start with flash bootloader first, what is ways for that?

 

Labels (1)
0 Kudos
Reply
36 Replies

7,575 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

Please create another ticker talk about this new question.  Thanks!

B.R

0 Kudos
Reply

7,657 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

you can find this all change in the i.MX Linux User's Guide file

B.R

0 Kudos
Reply

7,637 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

I followed that only and at last getting below logs while flashing flash.bin, it is getting stuck after 100%

U-Boot SPL 2022.04-dirty (Jan 07 2025 - 14:36:27 +0530)
Normal Boot
ELE firmware version 1.0.0-344acb84
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.17
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0:  RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x&88000000, size 288
Download 943104, Total size 944128
NOTICE:  BL31: v2.8(release):lf-6.6.3-1.0.0-0-g8dbe28631
NOTICE:  BL31: Built : 17:57:56, Jan 22 2024
NOTICE:  upower_init: start uPower RAM service
NOTICE:  user_upwr_rdy_callb: soc=b
NOTICE:  user_upwr_rdy_callb: RAM version:12.17


U-Boot 2022.04-dirty (Jan 07 2025 - 14:36:27 +0530)

M33 Sync: OK
CPU:   i.MX8ULP rev1.2 at 960 MHz
CPU current temperature: 46
Reset cause: POR
Boot mode: Single boot
Model: NXP i.MX8ULP 9X9 EVK
DRAM:  2 GiB
Core:  47 devices, 25 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0
Loading Environment from nowhere... OK
[*]-Video Link 0 (720 x 1280)
        [0] display-controller@2e050000, video
        [1] dsi@2db00000, video_bridge
        [2] panel@0, panel
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated
switch to partitions #0, OK
mmc0(part 0) is current device
UID 0x3baf2bda,0xb74e39fc,0xc40c9992,0xb364aa92
Detect USB boot. Will enter fastboot mode!
Net:   Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for                                mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo ;
Hit any key to stop autoboot:  0 

## Checking Image at 83800000 ...
Unknown image format!
Run fastboot ...
auto usb 0
No USB device found
USB init failed: -19
=> 
0 Kudos
Reply

7,633 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

One more IMPORTANT thing is in EVK there is typeC for flashing and we are using normal USB 2.0, do we require to change anything in configuration for that?

0 Kudos
Reply

7,662 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

Please refer our i.MX Linux User's Guide file compile the flaash.bin by yourself. Sorry about it. Because i can not help you compile it each time.

B.R

0 Kudos
Reply

7,661 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

That's completely fine zhang, Just share me imx-mkimage folder with all changes that you did I will generate flash.bin by myself.

0 Kudos
Reply

7,679 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

Please use the attachment flash.bin try again.

B.R

0 Kudos
Reply

7,664 Views
dhruvinrajpura
Contributor III

Hello @pengyong_zhang 

Thanks for sharing, In the Custom board we are using same UART port(lpuart5) with different pins, Can you share me updated flash.bin with below change in dts file

	pinctrl_lpuart5: lpuart5grp {
		fsl,pins = <
			MX8ULP_PAD_PTE6__LPUART5_TX	0x3
			MX8ULP_PAD_PTE7__LPUART5_RX	0x3
		>;
	};
Tags (1)
0 Kudos
Reply

7,735 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

please share me yout pass timing.c file i will help you generated the flash.bin, and see if it can pass.

B.R

0 Kudos
Reply

7,716 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

Attaching timing.c file for reference,

0 Kudos
Reply

7,870 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

After changing C12 from 3 to 1 I am able to calibrate my DRAM successfully,

>>>C12?

Is this issue reflects my previous change or it is something else?

>>>What is your next step when you generated the new timing.c file with DDR Stress tool? you should use it to replace the old timing.c file and re-compile the Uboot. then flash it to your board.

B.R

0 Kudos
Reply

7,760 Views
dhruvinrajpura
Contributor III

IMPORTANT,

Hello @pengyong_zhang 

Here I am attching updated logs, Earlier I was using only 1 bank for LPDDR, now I am using all existing configuration and generated timing file and created flash.bin and enabled debug log in u-boot I am attaching for reference, Can you tell me why log is like this?

0 Kudos
Reply

7,854 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

Updated Logs,

Is below issue can happen because of wrong ddr calibration or is this indicating different one?

 

U-Boot SPL 2022.04-dirty (Jan 02 2025 - 19:23:58 +0530)
Normal Boot
ELE firmware version 1.0.0-344acb84
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0:  RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot
Can't found uboot image in 640K range
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

 

0 Kudos
Reply

7,868 Views
dhruvinrajpura
Contributor III

@pengyong_zhang 

I exactly did same, I updated timing.c file and recompiled u-boot, took u-boot.bin and u-boot-spl.bin updated in imx-mkimage/iMX8ULP, generated flash.bin and flashed on board with uuu.

After that I am getting just below logs in my custom board and than failed,

U-Boot SPL 2023.04-dirty (Jan 02 2025 - 17:24:28 +0530)
Dhruvin
Normal Boot
ELE firmware version 1.0.0-344acb84
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0:  RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot

 

Just for reference in the EVK when I flash with it's compaible flash.bin logs were like

U-Boot SPL 2023.04+gf8a2983ec8+p0 (Mar 04 2024 - 07:25:04 +0000)
Normal Boot                             
ELE firmware version 1.0.0-344acb84     
upower_apd_inst_isr: entry              
upower_init: soc_id=48                  
upower_init: version:11.11.13           
upower_init: start uPower RAM service   
user_upwr_rdy_callb: soc=b              
user_upwr_rdy_callb: RAM version:12.18  
Turning on switches...                  
Turn on switches ok                     
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0:  RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x88000000, size 288
Download 999424, Total size 1000448
NOTICE:  BL31: v2.8(release):lf-6.6.3-1.0.0-0-g8dbe28631
NOTICE:  BL31: Built : 17:57:56, Jan 22 2024
NOTICE:  upower_init: start uPower RAM service
NOTICE:  user_upwr_rdy_callb: soc=b
NOTICE:  user_upwr_rdy_callb: RAM version:12.18

 

which is not coming in my custom board.

0 Kudos
Reply

7,921 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @dhruvinrajpura 

There is no this list, And It is no rule about the DRAM vendor.

B.R

0 Kudos
Reply

7,906 Views
dhruvinrajpura
Contributor III

Hello @pengyong_zhang 

After changing C12 from 3 to 1 I am able to calibrate my DRAM successfully,

dhruvinrajpura_0-1735823763275.png

 

Than I taken code and added where I am creating image and tried to flash image where I get below logs and than stuck, Is this issue reflects my previous change or it is something else?

U-Boot SPL 2023.04-dirty (Jan 02 2025 - 17:24:28 +0530)
Dhruvin
Normal Boot
ELE firmware version 1.0.0-344acb84
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0:  RNG instantiated
Trying to boot from BOOTROM
Boot Stage: USB boot


In the EVK after last line logs were like

Find img info 0x88000000, size 288
Download 999424, Total size 1000448

 

this is not coming in my board what can be issue for this?

0 Kudos
Reply

8,050 Views
pengyong_zhang
NXP Employee
NXP Employee

hI @dhruvinrajpura 

We have not test with only one channel on the two channel DRAM. So, I think it's not possible。

B.R

0 Kudos
Reply

7,987 Views
dhruvinrajpura
Contributor III

Hello @pengyong_zhang 

Can you provide me any document where all supported lpddr4/4x for IMX8ULP/IMX8ULP-EVK9 is listed?

0 Kudos
Reply

8,311 Views
pengyong_zhang
NXP Employee
NXP Employee

HI @dhruvinrajpura 

 I have checked this parameters about your new LPDDR on the RPA table, It same with the MT53D512M32D2DS. So,I don't think there's any problem with that. No need update about it.

B.R

0 Kudos
Reply

8,294 Views
dhruvinrajpura
Contributor III

Hello @pengyong_zhang 

One question here, in the logs I observed that registers associated with Channel A has proper value I think some issues with Channel B,

 

Is there any way we can configure and complete calibration for only channel A, if yes can you share me that XLs and .ds file which only configure and calibrate for channel A

0 Kudos
Reply