USB touchscreen not working with iMX6 sabre

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB touchscreen not working with iMX6 sabre

2,120 Views
czur
Contributor III

Hi,

I am trying to get the waveshare 10" hdmi display/touchscreen working with iMX6q sabre board. I have Yocto Linux build running on the board, The waveshare display uses the HID multitouch driver, but the driver does not seem to be recognizing the touchscreen.

I can see the touchscreen listed in the lsusb command, I do not see any error message from usbhid driver either.

Does anyone have any suggestions? I have connected the touchscreen to the sabre board via a USB hub to the USB OTG

igorpadykov

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

1,522 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arun

please look on helpful links

TSLib with EETI eGalax capacitive USB Touch - efusA9 NXP i.MX6 - F&S Support Forum 
Configure input offset and scaling for USB touchscreen - Variscite Forums 
touch screen - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply