USB touchscreen not working with iMX6 sabre

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB touchscreen not working with iMX6 sabre

1,990 次查看
czur
Contributor III

Hi,

I am trying to get the waveshare 10" hdmi display/touchscreen working with iMX6q sabre board. I have Yocto Linux build running on the board, The waveshare display uses the HID multitouch driver, but the driver does not seem to be recognizing the touchscreen.

I can see the touchscreen listed in the lsusb command, I do not see any error message from usbhid driver either.

Does anyone have any suggestions? I have connected the touchscreen to the sabre board via a USB hub to the USB OTG

igorpadykov

标签 (2)
标记 (2)
0 项奖励
回复
1 回复

1,392 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Arun

please look on helpful links

TSLib with EETI eGalax capacitive USB Touch - efusA9 NXP i.MX6 - F&S Support Forum 
Configure input offset and scaling for USB touchscreen - Variscite Forums 
touch screen - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复