USB circuit review needed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB circuit review needed

跳至解决方案
3,444 次查看
teju
Contributor I

Hi,

I request a review of the USB circuits designed for the IMX.53. We intend using both the on chip USB's as hosts.

Thanks

Teju

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,212 次查看
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,212 次查看
LeonCraven
Contributor II

If you are running both as host ports, do you need to connect USB_OTG_VBUS and USB_H1_VBUS to +5V via an RC filter, or can it be left floating?

I can't find the purpose of the VBUS pin in the literature. I'm assuming it is only used by the OTG port when it can operate as either an A or B port; to detect when external VBUS is applied. Is that correct?

0 项奖励
回复
3,212 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Teju,

Just one recommendation. When we use our channels as hosts, we use to place current limiters at VBUS just to make sure the USB max current specification is not exceeded. You can find examples of this in our reference designs.

Best regards.

Jorge.

0 项奖励
回复
3,213 次查看
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

0 项奖励
回复
3,212 次查看
teju
Contributor I

Thanks for your time.

0 项奖励
回复