USB circuit review needed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB circuit review needed

Jump to solution
5,519 Views
teju
Contributor I

Hi,

I request a review of the USB circuits designed for the IMX.53. We intend using both the on chip USB's as hosts.

Thanks

Teju

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
5,287 Views
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

View solution in original post

0 Kudos
Reply
4 Replies
5,287 Views
LeonCraven
Contributor II

If you are running both as host ports, do you need to connect USB_OTG_VBUS and USB_H1_VBUS to +5V via an RC filter, or can it be left floating?

I can't find the purpose of the VBUS pin in the literature. I'm assuming it is only used by the OTG port when it can operate as either an A or B port; to detect when external VBUS is applied. Is that correct?

0 Kudos
Reply
5,287 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Teju,

Just one recommendation. When we use our channels as hosts, we use to place current limiters at VBUS just to make sure the USB max current specification is not exceeded. You can find examples of this in our reference designs.

Best regards.

Jorge.

0 Kudos
Reply
5,288 Views
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

0 Kudos
Reply
5,287 Views
teju
Contributor I

Thanks for your time.

0 Kudos
Reply