USB circuit review needed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB circuit review needed

ソリューションへジャンプ
5,578件の閲覧回数
teju
Contributor I

Hi,

I request a review of the USB circuits designed for the IMX.53. We intend using both the on chip USB's as hosts.

Thanks

Teju

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
5,346件の閲覧回数
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,346件の閲覧回数
LeonCraven
Contributor II

If you are running both as host ports, do you need to connect USB_OTG_VBUS and USB_H1_VBUS to +5V via an RC filter, or can it be left floating?

I can't find the purpose of the VBUS pin in the literature. I'm assuming it is only used by the OTG port when it can operate as either an A or B port; to detect when external VBUS is applied. Is that correct?

0 件の賞賛
返信
5,346件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Teju,

Just one recommendation. When we use our channels as hosts, we use to place current limiters at VBUS just to make sure the USB max current specification is not exceeded. You can find examples of this in our reference designs.

Best regards.

Jorge.

0 件の賞賛
返信
5,347件の閲覧回数
Yuri
NXP Employee
NXP Employee

I do not see "criminals" on the scheme, assuming the i.MX53 OTG will be always used in host mode (ID is grounded).

0 件の賞賛
返信
5,346件の閲覧回数
teju
Contributor I

Thanks for your time.

0 件の賞賛
返信